Pumps, Fans and Compressors – The right spin of efficiency
Pumps, fans and compressors keep processes running in all industrial sectors. At the same time, these applications are typically the largest energy consumers in the plant, often their share is over 50%. Thus two things truly count: reliability – more than ever before – energy efficiency. And it is precisely here that Siemens drive systems stand out – for example, with savings of up to 60%.
Pumps, fans and compressors keep processes running in all industrial sectors. At the same time, these applications are typically the largest energy consumers in the plant, often their share is over 50%. Thus two things truly count: reliability – more than ever before – energy efficiency. And it is precisely here that Siemens drive systems stand out – for example, with savings of up to 60%.